Hi,
I am using a two stage LED driver solution. 1st stage is AC-DC and LM3450A is used for this. 2nd stage is DC-DC and LM3424 is used for that.
I am using eval boards for both these ICs for evaluation. LM3450A eval board outputs a 50V constant voltage that is used to drive LM3424. LM3424 is driving 9W LED bulb (30V @ 300mA). A PWM signal is used to control the LM3424 LED dimming.
When LED brightness is reduced gradually from 100% to ~ 10% by reducing the PWM duty cycle, the output current is not constant and LEDs start flickering.
What can be the reason for this? PWM frequency is 2kHz. I am doubting the minimum on time requirement of LM3424.
How to confirm this? And what can be a possible workaround?
Regards,
Vinod