Dear Friends,
I need to design a battery charge circuit for a portable device which equipped with two Li-Ion batteries. The input power is DC5V or USB power. Thank you.
Sunglin.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ti does not have any boost chargers to go from 5V to 8.4V. This would require a separate boost converter from 5V to at least 8.8V.
If you choose to do this then the charger portion would be the bq24133, bq24170, bq24120.