Hello All,
I'm facing an issue in getting TPS758A01LDO regulator to work, which i have implemented as per the below circuit from data sheet.
R1 = 39K, R2=27K. Co = 100uF (electrolytic). Vi = 5V. Expected Vout = 1.25 (1 + (39/27)) = 3V. (approx).
The thermal pad id connected the GND.
When the circuit is connected, the output voltage is 1.2V, and FB pin voltage is also 1.2V.
I have tried using different resistor values for R1 and R2, but still no change in the voltages.
Also the voltages are the same with load (100 ohm between Vout and GND) and without load.
Has anyone faced a similar issue. please help.
Regards
Hari