Hello, What is the best way to interconnect the fuel gauge BQ27510-G2 and the charger BQ24072? and I want to only use one battery pack thermistor for both IC's First can this be done if so how ? Or is it recommended to have two Thermistors in the circuit ? This is what I have so far (Please note I'm not a fully trained electronics engineer I'm only in training, so please excuse the messy layout and please feel free to point out any mistakes).
Circuit Info: Input Voltage via Mini-USB =5V Battery Voltage = 3.7V BQ24072: set to USB500 mode ISET= 450mA TMR= 3.5 Hours
Thank You And Hope Someone Can Help
Ben W