Other Parts Discussed in Thread: LM317, UC2834
I need a linear regulator that I can adjust the voltage and the current limit. less than 1 amp, about 15 volts out 40 vdc in
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LM317 is a good choice but the current limit is fixed. To get both an adjustable voltage and current limit you will need to use a LDO controller to control an external transistor. The UC2834 LDO Controller has an adjustable voltage and current limit.
could you provide some more info?
what's the maximum ambient operating temperature going to be?
Why 40V, will you be operating at this continually? 40V is quite high. 40V -15V = 25V x 1A = 25W = a lot of heat. A typical TO-220 part can only handle a couple of watts, so you may need a switcher.
I thinking of your heat dissipation here....