This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PoE PSE requirement

Other Parts Discussed in Thread: TPS2384, TPS23841

In looking through the lierature, it seems that I have an unusual requirement and I'd like some pointers/ideas.

The requirement is for a device with a single ethernet port to provide power to the port. The requirement is for 48V up to 100mA to be available. I could use the TI TPS2384 but that supports 4 ports and I only need one.

Also, any suggestions for a +12V to -48V conversion? It seems that most of the devices and/or designs are much heftier (1A or more!). In this application board space is at a premium and I'd like to keep it as small a possible.

Along the way I need to make sure that the design remains IEEE 802.3at (or appropriate letter) compliant.

Thanks