Other Parts Discussed in Thread: BQ25504
We are using bq25504 for energy harvesting application using solar input. We tried to replicate the circuit given in the datasheet on a breadboard. We did manage to get near datasheet values at intermediate nodes occasionally but eventually the IC stops working. We seem to have damaged 3 ICs over the last 2 weeks( The VBat pin, the VBat_OK,VBAT_UV,VBAT_OV pins show nearly 0 output). We would like to know where we are going wrong. We have not left the IC in no load operation and the input that we are getting from the solar panel is 1.2V, 150 mA.