Hello
My name is Amir and i'm using your charger in order to charge two series 3.8 volts cell (7.6 volts LI-ion prismatic) .
I have set charging voltage to 8.7 volts (according to battery spec). my problem occurs when battery voltage is about 7.8 volts and up to 8.7 volts: the charger does not start charging or it is starts after couple of seconds (can get even to 30 seconds).
If i am discharging the battery or putting load in the system and then set CE high, its start charging.
In voltages under 7.8 volts the charger starts and charging current is right according to ACSET and ISET that have planned.
Hope you can assist me.