I'm looking at the datasheet for TPS40060/61 and calculating component values. There is a section on MOSFET Switch Selection that uses the J/K method with equations and provides results for a design example. Unfortunately the equations use some terms that are not defined and the example does not show values for terms, only a result. It is not obvious to me where, in the TPS40060/61 electrical characteristics the numbers have come from for the undefined terms.
I don't see reference to an applications note and a search on the main TI web page for J/K does not return a result that answers my questions.
Can any of you direct me to good reference material?
Also, TI should fix an error in equation 20. The first two radicals have the 1/12 inside the Iripple^2 term.