P. 36 of the datasheet seems to indicate that the default value of the DEFCORE register (06h) is 14h/1Eh (depending on the value of DEFDCDC1). This would mean a default core voltage of 1.3V/1.55V instead of 1.2V/1.6V as stated on p. 22.
Is p. 36 correct or p. 22?
Also, if a resistor/divider is used to set the voltage, is this reflected in the DEFCORE register?