This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

any way in which we don't need REG to be configured ,just by setting the OTG pin high ,no need to configure REG in BQ24193

Other Parts Discussed in Thread: BQ24193

Hi All ,

I am evaluating BQ24193 as Battery charger IC. Its a Handheld application which would be capable of charging through USB2.0 and DC Adapter both.

I have a query regarding Boost Mode.In the datasheet it is mentioned we need to configure REG for Enabling OTG.

Is there any way in which we don't need REG to be configured ,just by setting the OTG pin high ,no need to configure REG after that.

When we will set the OTG pin as high ,it will go to Boost mode directly ,without any REG configuration.

Kindly reply asap.