Hi,
I have same problem than many people with the TPS40210. I understand that the step up with boost architecture have some limits but is quite easier to find inductance regards transformator. So, I have the same problème. My step up up to 90V is to near of limit duty cycle and with the slow switching time due to the low current gate driver, the mosfet switching disappear and give saturation coil. I would like to do a adjustable voltage regulator with current limiter but I don't find any sample schematic for that. Do you have please any experience or there is another chip better for that? I need 1A with 90V at 13V Vin.
Best regards
PS: Was be better to have a PWM limit and not Toff/Ton min because frequency dependance.
Also, add a current limiter possibility will be better (vs OC limit who switch off the power supply)