Hi,
We are debugging a 3rd party board which powers a SoC's 2.5V rail with a TPS63000 from a 5V input to the board.
We have noticed a high-speed(~ 5 MHz) transient glitch of 700 mV on the 5V to the TPS63000 shows up as a 1.5V pk-pk glitch( ~ 4-5 MHz)
at the 2.5V output. Just wondering if such behavior is plausible under high speed transients on the 5V input to the TPS63000.?
Any pointers to better understand this issue will be much appreciated. Thanks.