I am using TPS62130 as a driver for an LED circuit. I am having trouble with the switching. As I try to operate this there is no voltage on the output and there is no switching on pins 1, 2, 3. I have read that there are known problems with this chip. Are these problems still ongoing or have they been resolved? I will attach the schematic to see if I have other problems.7002.Schematic Design_ 4001188A00-00-REVD.pdf