This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL536A fault signals without uC

Other Parts Discussed in Thread: BQ76PL536A, BQ34Z100

Hi team,

 

How much functionality does the BQ76PL536A lose with the absence of a uC in the system? More specifically, how are the error flags (FAULT signals, etc) read out without a host? How is the EPROM programmed/read?

 

(The system is the BQ76PL536A + BQ34Z100). Here, the PL536A is more like an AFE without a controller.

 

Thanks for the help,

Yvette

  • There are two ways to detect fault.

    1. You must have FAULT_H pin connect toe 34Z100.

    2. Z100 must have SPI communitcation.

     

    Bottom line, PL536 is host mode. you must have uC with PL536. 

    You can't read out without host.

     

  • Hi Roger,

    Thanks for the reply. Just to clarify:

    -The z100 + p536 set up requires a microcontroller for reading out fault signals.

    -For this set up: the pl536's FAULT_H pin is connected to the z100. Then the z100 communicates with the microcontroller through SPI? The z100's data sheet mentions nothing of SPI communication. I did see I2C mentioned.

    Is this correct? Thanks.

  • Currently, Z100 can't communicate with PL536. As you mentioned above, PL536 is SPI communication which Z100 doesn't support.

    As of today, Z100 can't work with PL536.

    We don't have Z100+PL536 solution.

    We have Z100 solution with PL9XX.