Dear Sir/Madam,
I would like to know the power consumption of the TLC59116 when the oscillator is not running : Icc max value when bit4 is set in MODE1.
best regards
Sébastien Judenherc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Madam,
I would like to know the power consumption of the TLC59116 when the oscillator is not running : Icc max value when bit4 is set in MODE1.
best regards
Sébastien Judenherc
Sébastien,
The OSC bit will result in reduction of ICC by 2mA to 4mA. There are several other blocks in the TLC59116 that remain on and account for the remainder of the current.
Regards,
Dick