This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I want ESR vs Load Current graph for TLV70033.

Dear TI-er.

I saw that Datasheet is ESR Requirements for TLV70033.

My customer request ESR vs Load Current graph for TLV70033 .

plz help me.

  • Hi Kiyoung,

    The customer should choose the output capacitor with an ESR less than 200m ohm and a effective capacitance of 0.1uF. This ensures stability for all loads up to 200mA.

    The TLV70033EVM uses 1uF 0805 20% X5R 25V ceramic capacitors. This EVM is good example of a working design.

    The customer can order an EVM and test the TLV70033's performance with your application.

    Regards,

    Darwin