Hi!
I'm using a BQ2004E in one circuit, and when I was reading its datasheet, I had one doubt.
It says on page 4 that the range for fast charge work is V_HTF < V_temp < V_LTF .
But on page 5, it says that deltaT/deltat termination is only valid when V_tco < V_temp < V_LTF, so, out of that range the fast charge is cut if V_temp falls 16mV +-4mV. This range should be not like on page 4 (V_HTF < V_temp < V_LTF) ?