Dear all,
I have experienced a problem for some PCB's when trying to do a pack current calibration. I have a setup according to SLUA404 page 283 and i have followed the calibration instructions given on page 201-202 in the same document carefully.
When starting current calibration (2A through the 10 mOhm resistor) DFETD became set. With an AFE SC Dsg setting 12 the SCD bit was also set when starting current calibration, When changing the AFE SC Dsg to 72 SCD did not became set, - only the DFETD. I had to perform a 2673 1712 comand and a MAC 0041 command to get DFETD cleared. I increased the FET Fail Time from 5 to 10. That did not have any effect. The only way to avoid this was setting Fet Fail Time to 0 (disable).
I think I have seen others on the E2E describing a similar problem.
What could possible cause this problem ?
Best regards
Kjell