Hi,
We are working in a sensor nodes that aim to be similar to that it is shown in http://www.ti.com/lit/ml/slyt472/slyt472.pdf. It is intended to make use of the depicted devices, but we are having some questions about BQ25504?
1. Which are the differences between BQ25504 and a typical battery charger such as Bq24XX? The functioning principle is the same, in fact, both are battery chargers. The single difference is that BQ25504 can be powered from a lower voltage source, is this true?
2. In order to be powered a microcontroller from this kind of Energy harvesting device, is it needed a regulator(DC-DC conveter)? It will be well suited TPS6220x in combination with BQ25504? which one is well suited?
3. If there is no input source, the microcontroller will make use of the battery without worrying about the input source?
Regards.