This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78PL116 SpecificationInfo(0x1A) setting

Other Parts Discussed in Thread: BQ78PL116, BQWIZARD

Dear TI FAE

I had refer sluu481 document, the following description was copy form chapter 5.1.12

Bits 12 to 15 (IPScale) are set to 0000 by default by the bq78PL116. These bits can be set to 0001
through a Pack Configuration File (.tmap) generated by the bqWizard.

My application is 150A peak current for engine start BMS.

Can I set the IPScale for high current application?

My bqwizard is 3.2.0.0, does TI bqwizard have new version?

Best Regards.

CC Chen.