hi,
i intend to use the BQ24170 for application that need about 10-8W or higher, the thing is that i intend to use FET like IRLHS6242PbF at the input * 2, and CSD25401Q3 for the battery output.
if across the application i will have current of 4A through the input FET and 4-5A from battery during discharge, can i use the SMT FET or do i need larger one (like D-PACK) with heat sink.
can i relay on the thermal pad at the PCB for heat dissipation?