This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430 – The recommended value of FB resistor

Guru 21045 points
Other Parts Discussed in Thread: TPS5430

I would like to ask a question.

A customer is going to use R1=10.2kohm and R2=1.5kohm in the following condition.

Is this value the optimal?

Also,what is the reason the recommended values of R1 are 10kohm?

(detasheet P15 [For any TPS5430 design, start with an R1 value of 10 kohm.])

 

<Condition>

Vin= 12.5V

Vout= -9.5V

Iout= 0.8A

*Inverting buck-boost regulator