I cannot generate a senc file for the BQ34Z100. I always receive a communication error using either the eval board or the target hardware. I have no trouble writing a senc file into the BQ34Z100. Any help would be appreciated.
Thanks
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks. One more question. Is the state of health register strictly a decrementing value? I have new cells that are not indicating 100% even after a learning cycle.
The SOH is FCC / DesignCapacity, so it can increase if FCC increases. The device does not update DesignCapacity, so maybe the value is set too high.