Hi,
I am investigating TPS62170 buck regulator stability related to various input filters and for this purpose I would like to derive a rough approximation of the converter loop gain.
I've read SLVA463 (Optimizing the TPS62130/40/50/60/70 Output Filter) and I'm struggling to interpret the Loop Gain plots in Figure 3. The Gain looks pretty much like a second order system with it's corner frequency close to 1/(2*pisqrt(LC)) which is the corner frequency of the output filter. This makes sense to me since according to the book Fundamentals of Power Electronics by Erickson (p. 327) the loop gain is defined as:
T = H(s)*G_c(s)*G_vg(s) / V_M = X(s)*G_vg(s)
where H(s) and V_M are supposed to be constants and G_vg(s) is the open-loop transfer function v_o / v_i derived from a small-signal model of the converter. From the small signal model of the converter G_vg(s) can be approximated as the second order filter formed by the L-C output filter which leaves the term X(s) = H(s)*G_c(s) / V_M unknown.
However since G_vg(s) is a L-C low-pass the loop gain plot suggests some nearly constant gain amplitude for X(s).
Now, what I don't understand is the phase plot which roughly is a shift from 112° to -112° (or +90° to -90° for a even more optimistic approximation). G_vg(s) alone would clearly give a phase shift from 0° to -180° which leaves me puzzled what kind of transfer function for X(s) gives +90° to 0° phase at constant gain.
Thanks for any tips,
Arne