Hi,
We'd like to use the TPS61175 to boost our input voltage (3 to 4.2V) to Vout=12V. We used the webench tool (file attached) to define the external parts.
The point is that we're not happy with the specified inductor (Bourns SRN8040-6R8Y) since we have height restraints in our product.
We found an inductor (Vishay Dale IHLP2020BZER6R8M01) with the same inductance and similar rated currents. The main difference seems to come from the DCR which is around 150mohm for the vishay and 33mohm for the Bourns.
What could be the effect of such a DCR difference? I precise that our application is very intermittent: the TPS61175 will run 2*100ms a day....
Thanks for your help,