This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
on page 4 we can see the accuracy depending on the output voltage for LM3670.
I do not see why for the 3.3Vout we see -6% max whereas for the other output values the accuracy is closer to -4% or -4.5%. Could you please help to understand?
Thanks!
I have forwarded it to the MDP engineer for support.
Hi Leon, unfortunately this may be associated with "mask" option. That is when mask(s) are changed to realize another voltage option it may involve the feedback resistor hookup, compensation components hookup, and possible other current and voltage protection circuit change that occasionally results in layout or parasitic issue that impacts the accuracy as later validated during device characterization. Hope that helps explain some potential culprit involved. Regards, Kern