Any of you can suggest me an IC to design a battery charger for battery rating of 60 V, 120 Ah, lead acid. using CC and CV method ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We do not have any application notes for this high of voltage, but one could use the bq2031 with a power stage rated for 100V with the appropriate current rating.
There is no support for this unless the volumes are greater than 100k/yr and then it would go to a special solutions group that does custom designs for consideration.
This would require a very experience power supply engineer that could design the interface between the low voltage controller and the high voltage power stage.