This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

efficiency vs switching frequency

Other Parts Discussed in Thread: TPS54340

I am using TPS54340 in my project. according to its datasheet if I am using higher switching frequency then efficiency of the system will goes down and vice versa. but as i know that with high switching frequency, efficiency of the system goes high. please let me know how it is there?

  • Hi Ankush,

    The WEBENCH model for the TPS54340 is a good starting point to estimate what happens when changing the switching frequency. This efficiency in this model matches well with a real circuit.

    The largest change in power loss with switching frequency are switching losses. The loss can be estimated with equation 50 on page 33 of the datasheet. This equation shows a direct relationship between switching frequency and switching power losses. In other words higher switching frequency increases switching losses while a lower switching frequency decreases switching losses.

    Let me know if this helps answer your question.

    Best Regards,
    Anthony

  • thanks anthony,

    i have seen the webench model. with that i have simulated different designs for my different requirement.

    when i was working on it, one more surprising thing was there, when i am increasing the input voltage range, keeping all other parameter constant effeiciency of the system decreases. why is it so?

    for example 1st i designed for 14-20V input volt and 5V, 3.5A output rating for maximum efficeiency, then efficiency was higher. when i designed for 14-30V input range efficiency comes down? why is it so? can you please explore on it?

     

    thanks in advance,

    with regards,

    ANkush agrawal

  • With all other variable constant, efficiency decreases with higher input voltage.  That is due to switching losses in the FETs.