This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can not calibrate BQ3060 with advanced bqmtester

Other Parts Discussed in Thread: BQMTESTER, BQ3060

Hello, I'm trying to program and calibrate a BQ3060 with the "Advanced bqMtester" soft, but I can't.

After I set up all the configuration, I start the procedure, after recognizing the device, when the soft try to calibrate it, an error occurs:

Error 5010: Gas gauge was not in Calibration mode / could not be put in calibration mode.

If I try other tests like setting only de serial number, It can not be done.

Do you have any idea of what happening? The hardware is well connected

Thank you