Hi,
I am working on a BMS design for a primary battery that uses a chemistry other than Li-ion. I would like to use the bq20Z65-R1 in this design as it offers many features in a single chip that I require (impedance track SOC, protection, and SHA-1). Looking at the datasheet, it appears that I could configure the part to track SOC correctly by loading in a custom derived set of tables and parameters. Is this correct or do I need to consider the two chip solution of the bq20Z80A and bq29312A?
Thanks in advance for any help,
Mark