[Q1]
Which parameter should I input into ΔIo_set?
[Q2]
I use ceramic capacitor 88uF(22uF x 4).
Should I input 88 into Co_ceramic?*
*Vp-p becomes [#DIV/0!] when I do not input Co_Bulk,
but Co_bulk does not input because I do not use it.
<Condition>
・Vin=12 or 19V
・Vout=1.85V / 1.045V / 0.995V / 0.945V
・Iout=6A(max)
・L=2.2uF
・Co=88uF (ceramic capacitor only 22uF x 4)
・D-CAP2 mode