Is there a users guide for the Fusion GUI tool?
Is there a button to export the schematics for the power rails which are designed within the tool?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There isn't currently a method for exporting the schematic section of the Design tool inside the Fusion Digital Power Designer. This is a limited schematic which just includes the values necessary to complete the configuration of the controller and/or driver. It is not all inclusive, refer to the individual device datasheets for a more complete component requirement overview.
There isn't a user's guide to the Fusion GUI in itself. There is a quick start section of the Using the UCD92xx Digital Point of Load Controller document that may be of assistance, it can be accessed from within the Fusion GUI itself from the dropdown menu, Help --> Documentation & Help Center, then click on the UCD92xx tab and the document can be found under Application Notes.
I realize that the tool does not generate a complete schematic but it does select specific parts for the calculations and it is difficult to open each part and locate its part number in order to transfer the calculated functionality to my schematic. Can you generate a BOM?