Im searching for a proper solar panel for my harvesting chip BQ25504.
Can anyone suggest me proper open circuit voltages that I should get to fix as a power source? the datasheet suggests that 3v, 400mW is max. So are these conditions to be met by the open circuit Voltage and current or am I allowed to buy a solar panel a little higher than these voltages such as 5V ?
it is my intention to use these chips in parellel so that inuput power to the system is more than 400mW so I hope I dont need to worry much about the o/p current of the solar penel since I can devide in among the parrel BQ25504 chips.
Could anyone please advice me as to how I could chose the best max voltage of my Solar panel for this specific IC?