Hi,
I'm trying to find a chart describing ripple rejection PSRR vs. frequency of the TPS79147 (fixed 4.7V ouput) and TPS79101 (adjustable output). Unfortunately, the datasheet only specifies these figures for the 1.8V and 3.3V output versions. There is mention of 70dB PSRR at 10khz, which is helpful, but the plots for the TPS79118 and TPS79133 seem to contradict this number. Does TI have such plots ripple rejection plots available for the two parts in question?
Thanks,
Martin