This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dissapperance of selection guides

Other Parts Discussed in Thread: TPS61220, LMR61428, TPS61030, TPS60150

Hi,

 I need a micropower dc/dc converter (from 3.0Vdc to 5.0Vdc max current 50 or 100mA) for a new design.

Not able to find the product selector after the latest website update.

Any suggestion for a P/N and/or a link to the selection page?

Jan

  • I think right now the Webench front end has the most comprehensive component selection.  Your next best option is Power Quick Search.  Are you looking for Vin = 3 V, Vout = 5 V at 100 mA?  Let me know.

  • Thanks John,

    And yes, I am looking for Vin=3v, Vout=5V at 100mA.

    It is for a pressure sensor, so needs to be clean.

    What is your suggested part?

    Jan

  • None of the devices I directly support will meet that spec (you will need a boost converter).  I'll take a look and see if anything suggests itself.

  • power quick search returns 39 options for charge pumps and dc/dc switching converters.  More option if you want a controller w/ external FETs or a module.  I would probably go with a converter or charge pump.  So it will depend on your other care abouts...(size, cost, efficiency, etc).

    Charge Pump (Inductorless)
    Part Number  
    Description  
    Iout (max) (A)   Vin (min) (V)   Vin (max) (V)   Vout (min) (V)   Vout (max) (V)   Iq (typ) (mA)   Pin/Package   Approx. Price (US$)  
    Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending
    TPS60140 Regulated 5-V Charge Pump Voltage Tripler With Low Battery Indicator 0.1 1.8 3.6 5 5 0.055 20HTSSOP 0.65 | 1ku
    TPS60141 Regulated 5-V Charge Pump Voltage Tripler With Power Good Indicator 0.1 1.8 3.6 5 5 0.055 20HTSSOP 0.65 | 1ku
    TPS60150 140mA, 5V Charge Pump in 2x2 SON 0.14 2.7 5.5 5 5 0.09 6SON 0.50 | 1ku
    TPS60151 140mA, 5V Charge Pump in 2x2 QFN 0.14 2.7 5.5 5 5 0.09 6SON 0.50 | 1ku
    TPS60111 Regulated 5-V High-Power Low-Noise Charge Pump DC/DC Converter 0.15 2.7 5.4 5 5 0.05 20HTSSOP 0.70 | 1ku
    TPS60132 Regulated 5V high Efficiency Charge Pump DC/DC Converter 0.15 2.7 5.4 5 5 0.06 20HTSSOP 0.70 | 1ku
    TPS60133 Regulated 5V high Efficiency Charge Pump DC/DC Converter 0.15 2.7 5.4 5 5 0.06 20HTSSOP 0.70 | 1ku
    TPS60110 Regulated 5-V High-Power Low-Noise Charge Pump DC/DC Converter 0.3 2.7 5.4 5 5 0.05 20HTSSOP 0.80 | 1ku
    TPS60130 Regulated 5V high Efficiency Charge Pump DC/DC Converter 0.3 2.7 5.4 5 5 0.06 20HTSSOP 0.80 | 1ku
    TPS60131 Regulated 5V high Efficiency Charge Pump DC/DC Converter 0.3 2.7 5.4 5 5 0.06 20HTSSOP 0.80 | 1ku

    Back to Top



     
    29 Results   
    Converter (Integrated Switch)
    Part Number  
    Description  
    Design Software   Iout (max) (A)   Vin (min) (V)   Vin (max) (V)   Vout (min) (V)   Vout (max) (V)   Iq (typ) (mA)   Switch Current Limit (typ) (A)   Switching Frequency (max) (kHz)   Pin/Package   Approx. Price (US$)   Regulated Outputs (#)  
    Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending Sort Ascending  Sort Descending
    TPS61251 3.5MHz, 1.5A Current Limit, 92% Efficient Boost Converter for Battery Backup Charging 2.3 6 3 6.5 0.03 1.5 3500 8WSON 1.60 | 1ku 1
    TPS61252 3.5MHz, 1.5A, 92% Efficient Boost Converter with Adjustable Input Current Limit 2.3 6 3 6.5 0.03 1.5 3500 8WSON 1.25 | 1ku 1
    TPS61220 TPS61220 0.2 0.7 5.5 1.8 5.5 0.005 0.4 2000 6SC70 0.65 | 1ku 1
    TPS61222 Tiny Low Input Voltage Boost Converter 0.2 0.7 5.5 5 5 0.005 0.4 2000 6SC70 0.65 | 1ku 1
    TPS61093 Low Input, 20V/1.1A Step-Up DC/DC Converter with Integrated Power Diode and Input/Output Isolation 0.3 1.6 6 1.6 17 0.9 1.1 1200 10SON 1.30 | 1ku 1
    TPS61070 Adjustable, 600-mA Switch, 90% Efficient PFM/PWM Boost Converter in ThinSOT-23 0.5 0.9 5.5 1.8 5.5 0.019 0.7 1200 6SOT 0.80 | 1ku 1
    TPS61071 Adjustable, 600-mA Switch, 90% Efficient PWM Boost Converter in ThinSOT-23 0.5 0.9 5.5 1.8 5.5 0.019 0.7 1200 6SOT 0.80 | 1ku 1
    TPS61072 Adjustable, 600-mA Switch, 90% Efficient PFM/PWM Boost Converter in ThinSOT-23 0.5 0.9 5.5 1.8 5.5 0.019 0.7 600 6SOT 0.80 | 1ku 1
    TPS61073 Adjustable, 600-mA Switch, 90% Efficient PFM/PWM Boost Converter in ThinSOT-23 0.5 0.9 5.5 1.8 5.5 0.019 0.7 1200 6SOT 0.80 | 1ku 1
    TPS61170 1.2A Switch, High Voltage Boost Converter in 2x2mm QFN Package 0.96 3 18 3 38 2.3 1.2 1200 6SON 1.40 | 1ku 1
    Part Number  
    Description  
    Design Software   Iout (max) (A)   Vin (min) (V)   Vin (max) (V)   Vout (min) (V)   Vout (max) (V)   Iq (typ) (mA)   Switch Current Limit (typ) (A)   Switching Frequency (max) (kHz)   Pin/Package   Approx. Price (US$)   Regulated Outputs (#)  
    LMR64010 SIMPLE SWITCHER 40Vout, 1A Step-Up Voltage Regulator in SOT-23 1 2.7 14 3 40 2.1 1.5 1600 5SOT-23 0.60 | 1ku 1
    TPS61027 5-V Output, 1.5-A Switch, 96% Efficient Boost Converter w/ LDO Down-Mode, QFN-10 1.2 0.9 6.5 0.025 1.5 720 10SON 0.95 | 1ku 1
    TPS61202 0.3V Input Voltage Boost Converter with 1.3A Switches and 'Down Mode' in a 3x3 QFN 1.2 0.3 5.5 5 5 0.05 1.35 1250 10SON 1.10 | 1ku 1
    TPS61020 Adjustable, 1.5-A Switch, 96% Efficient Boost Converter with Down-Mode, QFN-10 1.2 0.9 6.5 1.8 5.5 0.025 1.5 720 10SON 0.95 | 1ku 1
    TPS61200 0.3V Input Voltage Boost Converter with 1.3A Switches and 'Down Mode' in 3x3 QFN 1.2 0.3 5.5 1.8 5.5 0.05 1.35 1250 10SON 1.10 | 1ku 1
    LMR62014 SIMPLE SWITCHER 20Vout, 1.4A Step-Up Voltage Regulator in SOT-23 1.4 2.7 14 3 20 2 2 1600 5SOT-23 0.55 | 1ku 1
    TPS61256 3.5-MHz High Efficiency Step-Up Converter In Chip Scale Packaging. 5V Output Voltage 1.9 2.5 4.85 5 5 0.02 2.15 3500 9DSBGA 1.30 | 1ku 1
    TPS61092 5-V Output, 500-mA, 96% Efficient Boost Converter, 20uA, QFN-16 2 1.8 5.5 5 5 0.02 2 700 16QFN 1.70 | 1ku 1
    TPS61085 18.5V, 2A, 650kHz / 1.2MHz Step-Up DC-DC Converter w/ Forced PWM Mode 2 2.3 6 2.8 18.5 0.07 2.6 8TSSOP
    8VSSOP
    0.95 | 1ku 1
    TPS61086 18.5V PFM/PWM High Efficiency Step-Up DC-DC Converter with 2.0 A Switch 2 2.3 6 2.8 18.5 0.07 2.6 10SON 0.95 | 1ku 1
    Part Number  
    Description  
    Design Software   Iout (max) (A)   Vin (min) (V)   Vin (max) (V)   Vout (min) (V)   Vout (max) (V)   Iq (typ) (mA)   Switch Current Limit (typ) (A)   Switching Frequency (max) (kHz)   Pin/Package   Approx. Price (US$)   Regulated Outputs (#)  
    TPS61090 2A Switch, 96% Efficient Boost Converter 2 1.8 5.5 1.8 5.5 0.02 2 700 16QFN 1.70 | 1ku 1
    LMR62421 SIMPLE SWITCHER 24Vout, 2.1A Step-Up Voltage Regulator in SOT-23 2.1 2.7 5.5 3 24 7 3 1600 5SOT-23
    6WSON
    0.75 | 1ku 1
    LMR61428 LMR61428 2.85 1.2 14 1.24 14 0.1 2.85 2000 8VSSOP 0.65 | 1ku 1
    TPS61175 3-A High Voltage Boost Converter with Soft-start and Programmable Switching Frequency 3 2.9 18 2.9 38 3 3.8 2200 14HTSSOP 1.80 | 1ku 1
    TPS61087 18.5V, 3.2A, 650kHz / 1.2MHz Step-Up DC-DC Converter with Forced PWM Mode 3.2 2.5 6 3 18.5 0.075 4 10SON 1.60 | 1ku 1
    TPS61253 3.5-MHz High Efficiency Step-Up Converter In Chip Scale Packaging. 5V Output Voltage 3.3 2.5 4.5 5 5 0.02 3.6 3500 9DSBGA 1.65 | 1ku 1
    TPS61030 TPS61030 3.6 1.8 5.5 1.8 5.5 0.02 4 700 16HTSSOP
    16QFN
    2.10 | 1ku 1
    TPS61032 5-V Output, 1-A, 96% Efficient Boost Converter w/20uA Iq in TSSOP-16 3.6 1.8 5.5 5 5 0.02 4 700 16HTSSOP
    16QFN
    2.10 | 1ku 1
    TPS55340 Integrated, 5-A 40-V Wide Input Range Boost/SEPIC/Flyback DC-DC Converter 5 2.9 32 3 38 0.5 6.6 1200 14HTSSOP
    16WQFN
    1.85 | 1ku 1

    Back to Top

  • John,

    Thanks for that comprehensive answer, appreciate it.

    Jan

  • It is quite a  list, let us know if one of those looks like a good fit for your project.

  • John,

    I need to do some comparison study between the charge pump (tps60150)

    and switch boost (tps 61222) and pick one of them.

    Thanks again.

    Jan