Using the LM25056Eval board we are not sure how to determine which Rs to use in order to measure current. We are also not sure if we should put this resistor across Vs+ and Vs-, on the Rs2 pads, or across, Rs+ and Rs-. Our input voltage ranges between 0 and 15 V, with a load resistor of 270 Ohms. We currently have Vs set to the default 30mV. When taking readings over the I2C bus we only get 0000.