I have a project that uses the TPS54620. I'm having every single one of these fail whenever break the input voltage with a switch, wire on a terminal, or push button and reapply it it dies. The inputs have been from 10v-15v, from lead acid batteries, bench top supplies, switchmode powersupplies. They don't all fail immediately some last longer than others yet 5 out of 5 have failed. They worked fine and regulated well enough when power is applied, I haven't had a chance to look at the waveforms but all of the circuits functioned properly so they must be pretty good and the output was within the expected range. Its just switching the power on and off kills. Vin,Vout, and GND are shorted together after failure. Quick reply would be greatly appreciated.