This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510 FLASH issue

Other Parts Discussed in Thread: BQ27510

Hello

I'd like to have infomation about BQ27510.

It had become a default value when FLASH data was checked.

Therefore, the data of FLASH considers that I would like to check the conditions which return to a default value.

Anyway my question is followings:

0)What is among the conditions from which FLASH data returns to a default value?  

 Is it, although I think that a RESET_DATA command (0x0005)  and the RESET (0x0041) command will correspond?

 

1)Although BQ27510 has Built-in FLASH, The default value is stored in some area,

 It returns to a default value by a specific command. Is it possible?

 

2)Can you teach the method, when "it can return to a default value"?

 

3)Although there is a RESET_DATA command (0x0005), when this command is used,  does the value written in by GoldenFile return to a default value?

 

4)Although there was the RESET (0x0041) command, when this command is used,

 What kind of operation does BQ27510 carry out?

 

5)When default data is stored in some area, If GoldenFile is written in,  what will happen to the default value?  Does a default value remain as it is?   Or does it write and replace by GoldenFile?

 Best Regards: Shing