This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24450 Current limiting

Other Parts Discussed in Thread: BQ24450

Hi,

I have got the Bq24450 to Work partially. I am using the following values

Battery: 12v 12Ah

Rc = 46k

Rd = 652k

Rb = 17k

Ra=493k

Rt = 1.33k

RISENS = 0.1ohm 3w

Rp = 1.9k

I am using a BD438 transistor and have a supply of 0-32v 2A and I would like to charge at 1A or as close to that as possible. Right now All I am getting is 40mA when the battery is connected, and 3mA when nothing is connected.

Can anyone advise me what to try next? 

Kind regards

Chris