This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G2 I2C Compatible with MSP430

Hello,

I'm trying to figure out if the Fuel Gauge BQ27510-G2 is compatible with the MCU MSP430FR5969. I'm having a little confusing because the BQ is a 2.5V device that feeds itself from the battery using its internal LDO, but the MCU is a 3.3V for which I have a different LDO for it. My compatible question is more specifically in the I2C lines, I'm not sure if Voh, Vol, Vih, Vil will be correctly detected. I have provided my schematics so far, it includes the fuel gauge and a battery charger.

Thank you!