This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Lower cost, larger package alternate device to LMR70503?

Other Parts Discussed in Thread: LMR70503, LM2611, LM2623

Hi Team,

Is there a device that has a larger package size, and lower cost, than the LMR70503?

Need to generate -1.5V supply from a 1.8V, 3.0V or 5.0V input at 10mA output current max.

Best Regards,

Shashank