Hi,
the maximum operating junction temp of LM5017 is +125 degrees C,
but in the description about thermal protection (D/S page11),
" the junction temperature does not exceed 150°C during normal operation."
does it mean that It's allowed to use LM5017 under the condition of the junction temp above +125 degrees C?
What does the "normal operation" mean?
Thanks,
Go