This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Soft Latch Power Switch



Hello

Sorry for the very Noob question but

I'm finding it hard to find a soft latch power switch IC which will connect to a single push button and will turn my system power on/off. Does TI have an SMD IC which can do this with minimal external components?

Or would I have to to it with MOSFETs and i few resisitors?

System specs:

Power source = 3.7V Li-ion battery (4.2V when charging)

I hope someone can help.

Ben W

Max current draw = 100mA