Hello,
I have tried to use the TPS61032PWPRG4 and have been unable to get it to function either on a breadboard or PCB. I am trying to implement a simple circuit to provide 5V, 1A from a Lithium Polymer battery.
My schematic is similar to Figure 19 "Power Supply Solution for Maxium Output Power" from the data sheet. Conponent values are:
C1=10uF ceramic
C2=2.2uF ceramic
C3=220uF tantalum
R1, R2, R6 = OC (I am not using the UVLO)
L1 = 6.8uH
I have connected LBI to PGND, FB floating, LBO floating. All other connections are per the schematic in Figure 19.
When I connect EN to VBAT I see about 1.75v on the output pins and the chip gets hot. VBAT is at 4.15v (full battery). I believe all connections are ok and have seen similar behaviour on breadboard and with some PCB's I have made.
Please assist, thanks.