Hi,
I have an application requirement that almost exactly matches the LM5118 Eval board;
Vin = 6 to 67V
Vout = 12V
Iout(max) = 3A.
I added some additional input circuit and designed a 2-layer version of the Eval board. This maybe my problem and I would appreciate some input!
Note: Component references are for my schematic, not the eval schematic.
For testing I have bypassed the additional input circuit; Vin is directly connected to C1-5 with a short length of 1mm2 wire. Vin is supplied from a bench PSU capable of 10A up to 15V and 5A up to 35V, the current limit is set to 10A.
I have the following problems.
- With no load, I have only 2V output at any input voltage up to 35V. This was improved by increasing the soft start capacitor from 100nF to 1uF. (Hint from another forum thread.)
- With the change in C17, Vout is 12V if there is no load. Vin immediately falls if a small load (470R) is connected to the output.
- Vout will only rise to 12V if Vin > 12V. Vin can then be reduced and Vout will remain at 12V (no load).