Hi,
Here is are some of the spec of what I need to build;
Input: 24 to 32
Output: +/- 12V @ 250mA
Ambient temperature: 150C to 175C
Application : Down hole oil drilling
I read a few post about making an inverting buck step down converter. I noticed that some of the IC are featured as inverting buck, but not those for temperatures above 150C. So I wonder if the inverting buck applies to any buck converter or if it's only certain of those that has that capability. If it's only certain of those that can, what are the specs that I have to look for to ensure that it does.
Thank You,
Ben