This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54425 / About the operation at the VREG5

Other Parts Discussed in Thread: TPS54425

Hi,

Now our customer is evaluating TPS54425 with forward configuration.

Please see actual waveform in attached.

Is this operation right?

8345.TPS54425_.pdf

yusuke

  • I have not seen that before, but in your case I think it is normal operation.  VREG5 is derived by linear regulator from Vin.  If you look closely, you can see that EN is rising slightly.  It is enough to temporarily enable the device.  VREG5 starts to regulate, but then EN returns to 0V.  VREG5 discharges.  After some time, EN is asserted high and VREG5 regulates to 5 V as it should.