This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

recommend ic

Other Parts Discussed in Thread: BQ24195

hi all, im still new here.

i'm looking for three type of ic.

basically, i'm trying to built  my own a portable power bank instead of buying ready made. the portable power bank basically consist of a parallel of 1 series li-ion battery, 4/5 led light for power capacity indication and charging status, 1 or 2 usb output for charging, 1 mini usb input for charging the power bank.

i'm electronic engineering student, so you can say i has some basic knowledge.

from my research, i think i need three type of ic, which is fuel gauge for capacity indication and also protection, charging ic for li-ion battery and also dc\dc convertion for li-ion to supply 5v constant dc volt. trying to built non-host power bank. there are so many type ic at TI, so i very hard to decide which one to select. and also, i need some help on the circuit.

for fuel gauge, i would love if it has 4-5 led indicator feature.

for charging ic, it would be best if it is 4.2V and max 1/1.5Amp.

for output of powerbank, i believe i found it, but need more suggestion xD. the one i found is pmp5417.