Hello,
TI has a Bridgeless 2 phase interleaved PFC kit, how is its EMI performance if compared with another TI kit:2 phase interleaved PFC?
Need to see if the bridgeless one does cause higher EMI in order to select one of them.
Thanks a lot,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
TI has a Bridgeless 2 phase interleaved PFC kit, how is its EMI performance if compared with another TI kit:2 phase interleaved PFC?
Need to see if the bridgeless one does cause higher EMI in order to select one of them.
Thanks a lot,
There is a 2 phase interleave PFC pre-regulator evaluation board using the UCC28070. The semi-bridge less PFC was an application note on how to design PFC pre-regulator. Neither of these were designed to meet EMI requirements. That being said we don't have EMI data on either.
You could order a UCC28070 interleaved EVM and measure the EMI and then modify it for semi-bridge less PFC and measure the EMI. When it comes to EMI the semi-bridge less should be the same as a single phase. When it comes to peak EMI I am guessing that they are probably about the same. Interleaved will operate at 2X the switching frequency and the noise spikes will have half the energy compared to the semi-bridgeless PFC. If you do take this data could you post in the forum so everyone can see it? I am interested to see what it is.
For interleaved PFC this is a 300W PFC pre-regulator and for semi-bridge less PFC it is a 150W design. That being said semi-bridge less PFC has a lower power density than interleaved PFC. Based on the size of the power stage, I would chose interleave PFC over semi bridge-less PFC.
Regards,
Hi Mike,
Thank you so much for the information,it is quite useful.I would try it and post the results as you suggested, it is quite interesting.
I do have more questions though:
1)UCC28070 is analog control , I'd like to try using digital control and TI has one by 28027. I suppose they are exactly the same in terms of power base board, the only differnce is just the controller, right?
2)Does TI have a ZVS PFC kit?
Thank you very much,